インフィニオン、世界最小の高周波用アンテナ向けESD保護ダイオードを発表
Technology Media
2008/11/11
ノイビーベルク/ミュンヘン(ドイツ)
独インフィニオンテクノロジーズは本日、「electronica」展示会において、最新の電子機器で使用されるアンテナの保護を目的とした、世界最小の過渡電圧抑制(TVS)ダイオードの提供を開始しました。主なアプリケーションには、GPS、モバイルTV、FMラジオ、車載用のリモート・キーレス・エントリ(RKE)やタイヤ空気圧監視システム(TPMS)が含まれます。新製品の「ESD0P2RF-02LS」は、実装サイズわずか0.62mm×0.32mm、高さもわずか0.31mmのTVSアンテナ保護ダイオードです。最新の電子通信機器や家庭用電子機器を静電気放電(ESD)から保護できるよう設計されており、最大20kVまでの静電気放電を確実に吸収できます。最大6GHzの高い直線性と、0.2pFというTVSダイオードとしては市場最小の容量、双方向型の構成での低制限電圧により、高感度高周波用アンテナ・アプリケーションに最適です。インフィニオンはダイオード技術で業界をリードしており、2007年12月にはすでに、高速データ回線の保護用として世界最小のTVSダイオードを発売しています。
TVSアンテナ保護ダイオードのESD0P2RF-02LSは、実装サイズわずか0.62mm×0.32mm(実装サイズ0.024インチ×0.012インチの0201インチ・パッケージに相当)のリードレスTSSLPパッケージ用に設計されています。同等の特徴を持つ既存製品と比べて約70%小さな小型パッケージとなっており、高密度PCB上での大幅な省スペース化と優れた柔軟性を実現するだけでなく、システム・モジュールやフロントエンド・モジュールのほか、フィルタやICのオリジナルの部品パッケージ(例:システム・イン・パッケージ、SiP)に直接集積できるよう特別設計されています。特に0.31mmの超低背パッケージは、携帯電話などの薄型ポータブル機器への実装で高い評価を受けており、どんなに厳しい高さ要件にも対応することができます。
インフィニオンのホルガー・ホマン(Holger Homann)(ディスクリート半導体事業ユニットTVS部門担当マーケティングディレクター)は次のように述べています。「新製品のESD0P2RF-02LSを使用することで、設計者は、システムレベルでのESDの堅牢性と信号品質のトレードオフを迫られることなく、アプリケーションの可能性を大きく広げることができます。TVS製品ファミリに新製品が加わったことで、インフィニオンは、超低容量の超小型TVSダイオードの先駆けとしての地位を、改めて確かなものとしています。」
超低容量特性
ESD0P2RFL-02LSダイオードの寄生容量はわずか0.2pFで、品質の劣化を伴うことなく、最適な信号品質と最高のESD保護を実現します。これによって、インフィニオンのダイオードは、0.5ns未満という超高速の応答時間を実現し、静電気放電電流を保護回路から安全な低レベルまで効果的に逃がします。これは、高周波用アンテナ・アプリケーションの非常に影響を受けやすい回路では、大きな価値のある特性です。ESD0P2RF-02LSダイオードのマルチストライクESD吸収能力は、接触放電で最大20kVであり、業界標準のIEC61000-4-2 level 4(8kV)を大幅に上回ります。
アンテナ保護ダイオードの新製品であるESD0P2RF-02LSは、GNDを中心に振幅する信号を扱うアプリケーション向けに設計されており、最大動作電圧は±5.3Vです。双方向対称な制限電圧特性により、PCB内のデバイスの配向性は問題となりません。最小1nA(5.3V時)という低リーク電流によってバッテリー持続時間の向上に貢献することから、バッテリー駆動のモバイル・アプリケーションは、この超小型TVSダイオードによって、極めて大きなメリットを享受します。ESD0P2RF-02LSは、車載向けのAECQ101規格などの、最も厳格な規格に適合しています。
供給状況
ESD0P2RF-02LSダイオードは、「ESD0P2RF-02LRH」ダイオードとともに、2008年内の量産開始を予定しています。ESD0P2RF-02LRHは、実装面積上の制限が少ないアプリケーションを対象としており、TSSLP-2より大型のTSLP-2パッケージ(1.0mm×0.6mm×0.31mm)で供給されます。TSSLP-2パッケージとTSLP-2パッケージはともに、RoHs及びハロゲンフリー指令に完全準拠しています。
詳細情報
インフィニオンでは、最新のTVSアンテナ保護ダイオードを、「electronica」展示会(ミュンヘン2008年11月11日~14日)においてデモ展示しています。弊社ブースはホールA5のブース#506です。インフィニオンのTVSダイオード製品ポートフォリオについての詳細は、
www.infineon.com/tvsdiodes
をご参照ください。
インフィニオンについて
インフィニオンテクノロジーズ(Infineon Technologies AG)は、ドイツのノイビーベルクに本社を置き、エネルギー効率、コミュニケーションズ、セキュリティという現代社会が抱える3つの大きな課題に対応する半導体およびシステムソリューションを提供しています。2007会計年度(9月決算)の売上高は77億ユーロ(キマンダの売上高36億ユーロを含む)、従業員は世界全体で約4万3,000人(キマンダの従業員約1万3,500人を含む)でした。インフィニオンは世界的に事業を展開しており、米国ではカリフォルニア州ミルピタス、アジア太平洋地域ではシンガポール、そして日本では東京の各子会社を拠点として活動しています。インフィニオンは、フランクフルトとニューヨークの証券取引所に株式上場されています。インフィニオンについての情報は次のURLをご参照ください。
本社サイト:
http://www.infineon.com
日本法人サイト:
http://www.infineon.com/jp
Information Number
INFIMM200811.008
| Press Photos | |
|---|---|
Image |
Description |
![]() |
The world's smallest transient voltage suppression (TVS) diode for the protection of antennas comes from Infineon. With a footprint of just 0.62 mm x 0.32 mm in size and a mere 0.31 mm in height, the ESD0P2RF-02LS diode is designed to protect the latest electronic communication and consumer devices against electrostatic overvoltages as high as 20kV.
|
![]() |
The world's smallest transient voltage suppression (TVS) diode for the protection of antennas comes from Infineon. With a footprint of just 0.62 mm x 0.32 mm in size and a mere 0.31 mm in height, the ESD0P2RF-02LS diode is designed to protect the latest electronic communication and consumer devices against electrostatic overvoltages as high as 20kV.
|
| Name | Contact | ||
|---|---|---|---|
|
Monika Sonntag Media Relations |
|