Energy Efficiency: Interview with Peter Bauer (CEO)

Mr. Bauer, suddenly everyone is talking about climate change – but mankind has an energy resource problem even without global warming, doesn’t it?

That’s right. Classical energy reserves such as coal and oil are finite. At the same time the global energy demand is constantly increasing, particularly in the national economies of the so-called emerging markets, including Asia’s two large countries China and India. This trend has caused energy prices to escalate in recent years. Intelligent solutions are now needed to cut down on costs, conserve resources and reduce the impact on the environment, and – as things stand at present – they can have only one aim: maximum efficiency.