Shareholder Structure
The number of shares held by Brandes Investment Partners, L.P., Capital Group International, Inc., Templeton Investment Counsel, LLC, Templeton Global Advisors Limited, Merrill Lynch International, AXA S.A. (incl. AllianceBernstein L.P.) and Dodge & Cox International Stock Fund is taken from the latest shareholder notification to Infineon and the respective authority. For more information please refer below to the reporting and disclosure requirements of shareholders.
total: 100 per cent = 749,742,085 (as of 2008-02-29)
| 100% Free float, of which: | |
|---|---|
| Brandes Investment Partners, L. P. |
3.08% |
| Capital Group International, Inc. |
4.14% |
| Templeton Investment Counsel, LLC |
4.89% |
| Templeton Global Advisors Limited |
5.16% |
| Merrill Lynch International |
5.25% |
| AXA S.A. (incl. AllianceBernstein L.P. with 4.76%) |
5.45% |
| Dodge & Cox International Stock Fund |
10.03% |
| Other shareholders (stake < 3%) |
62.00% |
(Status Shareholder Structure: as of 2008-12-04)
Disclosure Requirements for Shareholders
The German Securities Trading Act (Wertpapierhandelsgesetz) requires each person whose shareholding
reaches,
exceeds or, after exceeding,
falls
below the 3%, 5%, 10%, 15%, 20%, 25%, 30%, 50% or 75% voting rights thresholds of a listed corporation to notify such corporation and the German Federal Supervisory Authority for Financial Services (Bundesanstalt für Finanzdienstleistungsaufsicht - "BaFin") immediately, but no later than four trading days after they have reached, exceeded or fallen below such a threshold. For the purpose of determining the relevant shareholding, voting rights which are deemed to be held by way of attribution according to the rules of the German Securities Trading Act have to be taken into consideration. The violation of the disclosure requirement has serious consequences: Such holders cannot exercise any rights from those shares until they have satisfied this disclosure requirement. Besides, a fine of up to 200,000 euros can be imposed on the relevant shareholder.
Changes of Address in Share Register
Infineon shareholders can arrange online for a change in their address to be noted in the official share register (by clicking on "Shareholder" on the link below).
registrar services GmbH